EEO#.SOURCE

Description

This keyword sets the position source used to drive the EEO generator. The position source cannot use the same connector as the EEO connector.

SOURCE    
0 None  
1 to 5 Feedback FB#.P
11 to 12 Axis position feedback AXIS#.PL.FB
21 to 22 Axis position command

AXIS#.PL.CMD

Examples

Code

This command shows the allowed position sources for EEO1. Since EEO1 uses the X23 connector, which FB3 could have used, FB3 is not an allowed source.

-->DRV.HELP EEO1.SOURCE
Help for: EEO1.SOURCE [Integer] [NV] [ReadWrite] [Grouped]
Range: [1, 2, 4, 5]
Default = 1
Actual value = 1

This sets the first EEO instance to use FB2 as the source feedback.

-->EEO1.SOURCE 2

Context

For more information see Encoder Emulation.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units N/A
Range

0 to 5

11 to 12

21 to 22

Default Value 0 (None)
Data Type Integer
See Also  
Stored in Non Volatile Memory Yes

Variants Supported

All variants are supported.